Creating a common material library for all Solid Edge users

2021-10-06T23:54:43Z

Summary


Details

We are looking for the easiest way to make a single material library for all 
Solid Edge users. Currently all Solid Edge design engineers have their own 
Material Library with manually populated materials, but this is not an optimal 
practice.


We are looking for a solution which will allow all Solid Edge users to use a 
single material library managed through Teamcenter. Mapping all materials and 
their properties to Teamcenter is not as easy as it sounds, especially when 
they have to be available from Solid Edge Embedded Client. What is the best 
practice for creating and managing such a library?



Solution

Use the Solid Edge Material Library to distribute a consistent set of 
materials and associated physical properties to all designers. Physical 
properties such as mass, volume, surface area, material, accuracy, and density 
can be defined for use in the Teamcenter managed environment.


The best practice for implementing the exchange of the material, density, and 
accuracy properties in a managed environment is to set the property as owned 
by CAD, driving the design from CAD.


The Material.mtl can be placed on a shared network location and Solid Edge 
Clients can set in the Options -> file location the path to this centralised 
Material table.


Solid Edge physical properties such as mass, volume, and density can also be 
mapped. The following example specifies a Teamcenter Item Type of Document:


Material: ItemRevision.GRM(IMAN_master_form,DocumentRevision Master). 
SE_Material/master=cad/description="Material" 
Mass : ItemRevision.GRM(IMAN_master_form,DocumentRevision Master). 
SE_Mass /master=cad /description="Mass, Physical Properties" 
Volume : ItemRevision.GRM(IMAN_master_form,DocumentRevision Master). 
SE_Volume /master=cad /description="Volume, Physical Properties" 
Density : ItemRevision.GRM(IMAN_master_form,DocumentRevision Master). 
SE_Density /master=cad /description="Density, Physical Properties"



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEEC

Ref: 001-7918813

KB Article ID# PL8008998

Contents

SummaryDetails

Associated Components