Solid Edge Part text box with variable value not shown in drawing view

2021-10-06T23:54:41Z
DRAFT

Summary


Details

A Part Text Box with variable value is not shown in a drawing view.  Why?



Solution

The Text Box value is not shown directly on drawing, because it is an sketch 
annotation. 
Currently we do not show Annotations of e.g. a sheet metal/partfile in a 
drawing view directly.


It is possible to retrieve the Text Box via "Retrieve Dimension", but if the 
Text Box contains a variable value it is shown with "Error:No reference", 
because it is added as "From Active Document" Variable Property of the Sheet 
Metal Part model and this is not valid on the Drawing.


Workaround is creating the text box with the Variable retrieved from the 
Properties List "Named Reference" directly in the draft application. 
This value will be updated if it is changed in the model.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V109MP8
Function: DIMENSIONS

Ref: 001-8933445

KB Article ID# PL8008985

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS