How to control hole table labels, such as A1->A20 and B1->B5.

2021-10-06T23:54:40Z

Summary


Details

How to control hole table labels, where one table has holes 'A1->A20' and the other has holes 'B1->B5'.



Solution

1. Click on the first Hole Table. 
2. Click on the 'Notes and Tolerances' button. This is the icon which looks like a yellow page. 
3. For the Origin/size box, type "A". Click on the "Re-label List" button, then click on OK. 
4. Click on the next Hole Table. 
5. Click on the 'Notes and Tolerances' command. 
6. For the Origin/size box, type "B". Click on the "Re-label List" button. Then click on OK.

Please note: The above procedure is for the legacy hole tables created prior to ST10, or created using the "Legacy Hole Table" command by adding the appropriate icon to your command ribbon from the Customize dialog.

Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V109.0
Function: TABLES

Ref: 001-7920684

KB Article ID# PL8008977

Contents

SummaryDetails

Associated Components