When the customer tries to open a file - which is created in Solid Edge ST9 -
in NX 11 an error appears which says that "The part's file is saved in a newer
version, this one is not compatible with NX version"
The file is created with the ST9 with maintenance pack 1 and the NX 11 is the
last version too.
Is there some maintenance pack for NX 11 to solve this issue? Or
is there incompatibility with this version for some reason?
Solution
For Solid Edge ST9 file compatibility with the latest releases of NX and
Femap, the latest plmxml adapter may be needed and is available after ST9
release here:
https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/plmxml/
.
For NX, the adapter should be copied to the NX installation folder
(%UGII_BASE_DIR%\UGII).
For Femap, it should be copied to the Femap\Util folder.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: SOLID_EDGE
Application: TRANSLATORS
Function: OTHER
Ref: 001-7860686