Solid Edge Arrow break in weld symbol

2021-10-06T23:54:37Z
DRAFT

Summary


Details

How do you introduce an arrow break in the leader line of a weld symbol?



Solution

 If you want to introduce a break point in the leader line of a weld symbol do the following:


With the select tool active click the leader line so that it highlights. Then press the ALT key and click at the desired break location. This will add a control point in the leader line which can be dragged around.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DRAFT
Version: V109.0
Function: ANNOTATIONS

Ref: 001-7791982

KB Article ID# PL8008957

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS