Solid Edge Values in balloon tab of the Parts List Properties are grayed out.

2021-10-06T23:54:37Z
DRAFT

Summary


Details

Values in balloon tab of the Parts List Properties are grayed out.



Solution

Values in the Balloon tab of 'Parts List Properties' are available on create. When placing the parts list, click on the view, click on 'Properties' button in the Parts list toolbar and then click on the 'Balloon' tab. You will now have access to the values in the balloon tab. Once the list has been placed, these values are then disabled.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V109.0
Function: ANNOTATIONS

Ref: 001-8948651

KB Article ID# PL8008953

Contents

SummaryDetails

Associated Components

DRAFT: DRAWING_VIEWS