Issue registering SEPropertyhandler.dll file

2021-10-06T23:54:35Z

Summary


Details

In this scenario the user's 'Where Used' is not working and accordingly an attempt is made to register the SEPropertyhandler.dll to fix this but results in problems on the Windows 10 client. 


Steps to reproduce:


Run cmd prompt 
Type: cd C:\Program Files\Solid Edge ST9\Program\ 
Type: regsvr32 sepropertyhandler.dll


I receive the error although being local administrator on the client: 


'The module "SEPropertyHandler.dll" was loaded but the call to DllRegisterServer failed with error code 0x80070005.'


If I run the cmd window as usual (from 'search' or 'cmd' entered at the top of file explorer) I receive the error.



Solution

 You will need to open the cmd-prompt from the start-menu and 'RMB/run as admin' 
 - then you can register the dll.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP6
Function: SEDM

Ref: 001-8852786

KB Article ID# PL8008939

Contents

SummaryDetails

Associated Components