Want different neutral factors in same part in Synchronous.

2021-10-06T23:54:30Z

Summary


Details

Can you specify unique neutral factors per bend in Synchronous?



Solution

 Yes, this is possible both during placement and after placement.


During placement, (for example, when pulling a flange out from the edge of the 
part), you need to go to the Flange Options button on the command QuickBar. 
On the Options dialog, click the checkbox to override the global value, then 
the neutral factor field will become enabled and you can key in the desired 
value.


After placement, you will need to select the bend itself, then click on the 
callout pointing to the bend. On the QuickBar, you will select the Bend 
Options button, check "Override global value" next to the Neutral Factor and 
then enter the desired value.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: PART/SHEETMETAL
Version: V110.0
Function: FEATURES

Ref: 001-7894496

KB Article ID# PL8008909

Contents

SummaryDetails

Associated Components