How to add properties for use with Search in Windows Explorer.

2021-10-06T23:54:29Z

Summary


Details

How do you add properties for use with Search in Windows Explorer.



Solution

'Solid Edge Options -> Fast Property Search' is where most of the UI for Fast Search is located. There is a section for 'Custom Properties' to help you set up the Search.


'Set Custom Properties' enables the addition of the custom properties. 'View Custom Properties' lists them. If a value of 1000 for example is entered in a Solid Edge part file and you search in Windows Explorer for "custom2:1000", you can find that specific document. If you choose to add properties to 'propseed.txt', then those can be used to Search in Windows Explorer.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109.0
Function: SEDM

Ref: 001-7808291

KB Article ID# PL8008899

Contents

SummaryDetails

Associated Components