SE_Assembly_Construction pseudo folder is not created

2021-10-06T23:54:29Z

Summary


Details

How do I show a construction part in the SE_Assembly_construction pseudo 
folder?


My Teamcenter preferences are defined thus so that I can use reference/construction 
parts in a Teamcenter BOM and show in a pseudo folder:


SEEC_BOM_Synchronize = TRUE 
SEEC_Enable_AssemblyConstructions= 1


Steps to reproduce:


 1. Create an Assembly in Solid Edge and save. 
 2. Create in-place new part1. 
 3. Create in-place new part2. 
 4. Define "HigherLevel = No" and "PhysProps = No" for Part2 
 5. Save the Assembly and check in to Teamcenter.


In Teamcenter I do not see the SE_Assembly_Construction pseudo folder.



Solution

To show the SE_Assembly_Construction pseudo folder you have to configure the 
Rich Client first:


- In the RAC go to Edit -> Options 
- Select the left hand pane "General -> Item Revision" 
- Add the SE_Assembly_Construction to the "shown relations" 
- Go to the Related object tab 
- Add the SE_assembly_Constructions to the "Shown Relations"


Now the construction occurrence will show in the SE_Assembly_Construction 
pseudo folder.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEEC

Ref: 001-8311278

KB Article ID# PL8008898

Contents

SummaryDetails

Associated Components