Solid Edge Simulation - Mesh window is not shown

2021-10-06T23:54:28Z
SIMULATION

Summary


Details

In this scenario the Mesh window is not shown when the user clicks on the Mesh icon. 
When Solid Edge settings are restored to defaults (by manually deleting the registry entries) the Mesh window is shown normally. 
However the issue reappears.



Solution

If you define a folder for Nastran scratch directory and then you delete this folder, the folder is automatically created when needed. However If you do not have write access to the upper folder, the scratch folder is not automatically created when needed and this causes the issue with the Mesh window 
disappearing.


For example:


Set Nastran scratch directory to: C:\Users\demo\AppData\Roaming\Unigraphics Solutions\Solid Edge\SESimulation\


Then delete the folder \SESimulation\.


Solid Edge was not able to create a new \SESimulation\ folder because the logged in user has no write acces to the upper folder C:\Users\demo\AppData\Roaming\Unigraphics Solutions\Solid Edge\


The fix is to set the Nastran scratch directory to a different folder, where the user has write permissions.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: SIMULATION
Version: V109MP4
Function: ENVIRONMENT

Ref: 001-7968079

KB Article ID# PL8008893

Contents

SummaryDetails

Associated Components

SIMULATION: ALL