Import STEP to Solid Edge as assembly so that Part Copies become parts

2021-10-06T23:54:26Z

Summary


Details

When a STEP is imported as an assembly it may result in one part. However when you open 
the part there are a lot of Part Copies. User would like an option so that 
when this happens Solid Edge creates parts of the Part Copies. 


Is there an option in the STEP import options to create an assembly with parts when 
this happens?



Solution

Edit the Solid Edge program\preference\translators\STEP.INI and 
modify "Import Multiple Bodies As Single Part file=On" to Off. This will 
create a unique part file for each Solid Part copy



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: TRANSLATORS
Function: STEP

Ref: 001-8341665

KB Article ID# PL8008878

Contents

SummaryDetails

Associated Components