Solid Edge Relations for every item with a Solid Edge drawing is corrupting with each Save

2021-10-06T23:54:24Z
DOC_MANAGEMENT

Summary


Details

TCRS 11.2.0 has been patched to TCRS 11.2.3.


Relations for every item with a Solid Edge drawing is corrupting with each 
Save As action. This only occurs when many Teamcenter servers are active.


Steps to Duplicate: 
======================================== 
Create an SE Assembly with SE Parts. The parts have an SE Draft attached. 
In Solid Edge use the command: "Replace part with copy" 
Assign an Item ID and perform the action. 
In this case an error is returned: 


"The instance cannot be saved because it contains at least one attribute 
that violates a unique attribute rule."


The "Save As" action performed on the object "Test" has failed


The TALLOG states the following error. 
"Empty Typename passed to ConstructObject!!!! SEEC layer SHOULD pass 
Typename in this workflow"



Solution

The Compatibility mode of SQL Server 2014 should not be set to SQL 2014 (120) 
when the OS is Windows 2012R2 as this causes errors with copying (Save As, 
Replace with Copy etc.) corrupting the contents of the database. 
It is also slowing the server down by a factor of a hundred. It seems that 
querying the database has changed between 110 and 120. The compatibility mode 
has been set back to 2012 (110)


For more details:


https://social.msdn.microsoft.com/Forums/sqlserver/en-US/efc7958f-3481-4ac3-bc5 
4-ffd80ad07fc7/query-slow-in-sql-server-2014-vs-sql-server-2008-r2?forum=sqldat 
abaseengine



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEEC

Ref: 001-8332553

KB Article ID# PL8008866

Contents

SummaryDetails

Associated Components

DOC_MANAGEMENT: SEEC