SEEC does not check for duplicate folder defined by SEEC_Template_Folder_Name

2021-10-06T23:54:24Z

Summary


Details

If a second folder with the same name as defined in SEEC_Template_Folder_Name 
exists in the Home folder, SEEC is unable to download the managed templates.



Solution

In SEEC, after cleaning the local cache, the template files are not 
downloaded anymore and local templates are used instead.


In this case the user cut and pasted the "Solid Edge Templates" folder 
to the Newstuff folder of infodba. They then ran the "Import Solid Edge 
Templates" tool again to upload a new set of templates.


To fix this check the Home location defined in SEEC_Template_Username 
to see if a duplicate template folder exists. 


If a duplicate template folder exists delete or rename the duplicate 
template folder.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEEC

Ref: 001-7891101

KB Article ID# PL8008865

Contents

SummaryDetails

Associated Components