The customer is performing a 'Where used' action in Solid Edge or Design
Manager. He adds a NON-Indexed folder location to the search scope (red
folder). In the next dialogue he is prompted to add this folder to the Index:
'Some added folders are not indexed. This will slow down the search
performance. The local folders can be indexed now. Should Windows get them
indexed now?'
This is not possible because both options (Yes and No) are grayed out.
Solution
Check whether you have selected a network location and added this to
the search scope. If so you will be using only the local Windows search service
and will not be able to add this location to the search.
Notes and References
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEDM
Ref: 001-8328387