Subassembly in draft not updating correctly after adding part to subassembly

2021-10-06T23:54:23Z

Summary


Details

Create a Drawing View of a sub-assembly from an assembly that already has a Drawing View. 
In the Drawing View Wizard do not select the "Create drawing view independent of assembly".


The resulting new Drawing View will not show parts that are added to the sub-assembly. Why?



Solution

This is designed behavior that makes it possible to create a Drawing View of a sub-assembly in the context of the assembly so that any Parts List and Balloons will be the same across both views.


You can override the settings to remove the behavior described above by defining these options when creating the Drawing View:


1. In Drawing View Properties -> Model Options -> Assembly check - 'Show new components added to assemblies in drawing views'. 
2. In Drawing View Properties -> Display -> deselect 'Filter drawing view display list to display only shown components'.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: DRAFT
Version: V109MP5
Function: DRAWING_VIEWS

Ref: 001-8008975

KB Article ID# PL8008861

Contents

SummaryDetails

Associated Components