Chinese Solid Edge does not resolve the Project Name correctly

2021-10-06T23:54:22Z

Summary


Details

A customer has configured a Chinese Solid Edge/SEEC version to work with an 
English_US local Teamcenter environment. They have problems with attribute 
mapping - attributes are not synchronized.



Solution

Reviewing the TAL-log this message is seen at the top:


When trying new login, an InvalidCredentialsException was thrown. Message 
said: The requested locale (Chinese [zh_CN]) cannot be used by the Teamcenter 
server process. Connect in one of the following locales: English, French, 
German, Italian, Spanish, Portuguese. Alternatively, limit data entry to 
characters from one of these locales


locale problem; retry with en_US locale


This is because you are using a Chinese local to comunicate with a US database. 



Teamcenter does not support this on V10000.1.0.40_20150421.00 (which means they 
cannot consume the character data that we can create in Solid Edge) and you 
need to move to a supported language or upgrade to TC 11.2 AND implement UTF-8.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEEC

Ref: 001-8334537

KB Article ID# PL8008860

Contents

SummaryDetails

Associated Components