ST9 Free 2D does not contain Viewer to view 3D data

2021-10-06T23:54:18Z

Summary


Details

ST9 Free 2D does not contain Viewer to view 3D data.



Solution

The first workaround is to download the ST9 Maintenance Pack 1, however this is 
only possible if the customer is under maintenance.  Detailed information 
related to the fix and handling with ST9 MP1 can be found in SFB 002-7008852: 


http://uscisgtslrp001.industrysoftware.automation.siemens.com/view.php?sort=des 
c&dt=faq&q=ST9+viewer&file_type=html&i=002-7008852&k=1&o=0


In the case of not having maintenance the workaround is to download the Solid 
Edge Free Viewer, but not to start the executable to install the Free Viewer, 
because this will not work and bring up a message that Solid Edge is installed 
and needs to be uninstalled.


1. Extract the SE_Viewer_YOURCHOOSEDLANGUAGE_ST9.exe Application file to a 
temporary folder e.g. with 7Zip. 
2. Go to the "CD rom" Folder and extract "Execut~1.cab" e.g. with 7Zip 
3. Copy the now existing File "F20151_seviewer.exe" to the Solid Edge 
Program/win32 folder. 
4. Pin the Application to the Start or Task Bar to have it available to use.



Notes and References


Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: SETUP
Version: V109MP4
Function: INSTALL

Ref: 001-7955139

KB Article ID# PL8008830

Contents

SummaryDetails

Associated Components