User is using a Teamcenter naming rule with a counter in a custom property. In the Teamcenter RAC during the creation of a new Item they are able to assign a number to the custom property.
When attribute mapping is set up for Solid Edge Embedded Client (SEEC) the custom attribute will show up in the Custom Properties Dialogue. However the user is unable to assign a number to the custom property.
Solution
Secondary counters are not supported with SEEC. In SEEC only a number is assigned to the ItemID.
The workaround is to create the Item in Teamcenter first and assign the number to the custom property.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEEC
Ref: 001-8864385