How do I map the Cut Length of a frame part to my Teamcenter BOM?
This property is by default available in the Solid Edge Parts List.
Solution
There is no specific mapping required to show the frame cut length in the
Teamcenter Structure Manager. By default the individual length of each frame
part is written to the property "SE Cut Length" - the only action required is
to insert this column in the Teamcenter Structure Manager (Insert Column(s) ->
select SE Cut length in the available columns and add to the Displayed Columns)
In a Solid Edge Parts List you can also make the Total Length visual. This
option is not available in the Teamcenter Structure Manager. However Teamcenter
has an option to use Rollup reports for calculations based on the Teamcenter
BOM in Excel.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Function: SEEC
Ref: 001-8863981