'Angular Coordinate Dimension' is only showing degree symbol at zero.

2021-10-06T23:54:14Z

Summary


Details

'Angular Coordinate Dimension' is only showing degree symbol at zero.



Solution

When 'Units->Angular->Round-off' is 1, which is the default, the 'Leading' and 'Trailing' zeros properties are ignored. This will display the zero value for degrees. But if you have 'Units->Angular->Round-off', such as .1234 with 'Leading' and 'Trailing' zeros unchecked, it will result in a blank value at zero degrees. Hence, you will need to check those properties to display zero degrees.



Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: DRAFT
Version: V109.0
Function: DIMENSIONS

Ref: 001-8939788

KB Article ID# PL8008809

Contents

SummaryDetails

Associated Components