How to install Solid Edge CAM Pro 2019.

2021-10-06T23:54:11Z

Summary


Details

How to install Solid Edge CAM Pro 2019.



Solution

Installation of Solid Edge CAM Pro 2019

1. Download 'Siemens PLM Licensing -> Product Updates -> Installs -> SPLMLicenseServer_v9.1.0_win_setup.exe' from the GTAC web site: https://download.industrysoftware.automation.siemens.com/ 

2. Download 'Solid Edge -> Full products -> Windows (64-bit) -> 2019 -> CAM Pro -> Solid_Edge_CAMPro_2019.exe'. 

3. Double click on 'SPLMLicenseServer_v9.1.0_win_setup.exe'. Although there is a SPLMLicenseServer delivered with 'Solid_Edge_CAMPro_2019.exe', it is a previous version which leads to the error 'Could not find a valid Java virtual machine to load'. 

4. Continue with the 'Siemens PLM License Server v9.1.0' Setup Wizard. Keep or define the installation directory. Click on 'Next'.

5. Browse to the Solid Edge CAMPro license you received and click on 'Next'. You will be presented with a 'Pre-Installation Summary'. Click on 'Next'. You should get a message 'Install Complete'. Click on the 'OK' button and click on 'Finish'. 

6. Double click on 'Solid_Edge_CAMPro_2019.exe', accept the terms in the license agreement. Leave the 'License file' box empty, since it was part of the license server installation. Then click on 'Install'. The wizard will skip the "SPLM License Server Installation' and will go straight to 'Solid Edge CAM Pro Installation'. This takes a bit of time to complete. 

7. Once installed, start Solid Edge. Create or open a model and launch Solid Edge CAM Pro 'Tools -> Environs -> CAM Pro').  A 'Routing to application' message should come up and opens NX Version 12.

Notes and References


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: SOLID_EDGE
Application: SE_CAM_PRO
Version: V219.0
Function: OTHER

Ref: 001-9430371

KB Article ID# PL8008789

Contents

SummaryDetails

Associated Components