NX How to display reference designator as a column in Structure Manager

2021-10-06T23:26:38Z
NX for Design

Summary


Details

How to display reference designator as a column in Structure Manager.



Solution

In NX12.0.2, you must do the following two things:
1. In the %UGII_BASE_DIR%\UGPCBXCHANGE\psbx_ug_model.ini, set the following:
NxWriteTcUserRefDesProperty= yes 
2. In Teamcenter, under 'Edit-->Options', add "ReferenceDesignator" for the option: PS_structure_change_condition
Now when you import an IDX file, you can save it to Teamcenter.
In Structure Manager, make the Reference Designator column available to see the information.



Notes and References


Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: ATTRIBUTES

Ref: 001-9420017

KB Article ID# PL8008748

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX