Uninstalling Key Shot from Solid Edge

2021-10-06T23:54:08Z

Summary


Details

Can a user uninstall keyshot alone, as it is not required when a Foundation license is procured.



Solution

Uninstalling KeyShot has not been tried and tested and not valid use-case.
 
 
 
 However, technically it will uninstall without any issue and one can work in Solid Edge
 
 
 
 Just in case the end user faces any issue while using Solid Edge in future and report an issue to GTAC, 
It would be expected to retest the issue/query by having KeyShot installed and if the error persists then only will the issue/query will be addressed.




Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 10_1809
Product: SOLID_EDGE
Application: SETUP
Version: V219.0
Function: INSTALL

Ref: 002-8008725

KB Article ID# PL8008725

Contents

SummaryDetails

Associated Components