In the situation where a user has '
Mach 1' and '
Mach 3' license bundles selected (via the '
Licensing Tool - Bundle Settings' dialog):

The '
Mach 1' bundle will (typically) be checked-out when NX is started and 'core' modeling functions (such as Sketch and Extrude) are used. If the user then selects an 'advanced' function (for example 'X-Form'), then the '
Mach 3' bundle will be checked-out and the '
Mach 1' bundle checked-in. (This is known as Automatic Bundle Consolidation.)
However, after finishing with the 'advanced' command the specific license feature will be checked-in, but the '
Mach 3' bundle itself (and the core license features within the 'Mach 3' bundle) will remain checked-out, even though only core modeling functions are now being used. NX does not automatically 'downgrade' the user to the '
Mach 1' bundle, this is to ensure they can access the advanced features again, should they be required. If there are limited numbers of '
Mach 3' bundles, the user can choose to relinquish the '
Mach 3' bundle and revert back to '
Mach 1', using the procedure outlined below.
Solution
The user can manually switch back to the '
Mach 1' bundle (assuming one is available) and return the '
Mach 3' bundle, without exiting NX, using the following procedure:
1. Select the '
Application' tab, then '
More - Gateway' (at this point all the '
Mach 3' bundle features will be checked-in, except for the '
gateway' feature and the bundle itself).
2. Select '
File - Utilities - Select Bundles...', the Licensing Options dialog shows the '
Mach 3' bundle at the top of the list, because it is the bundle currently in use. Select the '
Mach 3' (NX13100N) bundle and use the down arrow to move it below the '
Mach 1' (NX11110) bundle. Select '
OK'.

3. On the '
Application' tab, select '
Modeling'. When a core modeling command is selected, for example 'Edge Blend' the '
Mach 1' bundle with be checked-out and the '
Mach 3' bundle is checked-in, making available to other users.
Notes and References
Hardware/Software Configuration
Platform: INTEL
OS: window
OS Version: 1064
Product: NX
Application: PLATFORMS
Version: V12.0
Function: FLEXLM
Ref: 001-9419651