More info about Create with Centerlines.

2021-10-06T23:26:38Z

Summary


Details

Problem:

While creating Views "Create with Centerlines" option is set as check ON, but some auto centerlines are not created for the cylindrical faces.

Solution

Auto CenterLines are created while creating Views for cylindrical faces which are complete 360 degree rotated. If it's not a 360 degree of cylindrical face, CenterLines  can't be created.


In this case, we need to create a CenterLines  after placing the view by  using the "Automatic CenterLines"  option


[Menu>>Insert>>Centerline>>Automatic]


1.Auto CenterLines are not created while creating the below View.
2.Auto CenterLines are created while creating the below View.3.CenterLines are created  by using "Automatic CenterLines"  option


Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: ANNOTATION

Ref: 002-8008692

KB Article ID# PL8008692

Contents

SummaryDetails

Associated Components