NX Information about edit the Hole Callout (Radial Dimension).

2021-10-06T23:26:38Z
NX for Design

Summary


Details

Problem:

There is a model that created multiple holes with one feature using the "Hole" command.
 In the Drafting, create dimension using "Radial Dimension" command set to "Method: Hole Callout".


 Is there a way to move this created dimension to another hole?

Solution

Hole Callout Dimension is the feature Based dimensions, so we can't have move this created dimension form one to another hole, but we can move the dimension from one feature hole to another feature hole and back to original feature hole in a required location.
 
OR user can delete existing Hole Callout Dimension and recreate Hole Callout having a new location.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: DIMENSION

Ref: 002-8008688

KB Article ID# PL8008688

Contents

SummaryDetails

Associated Components

Drafting