When Extruding a one degree Spline, a Convergent body is the result

2021-10-06T23:26:38Z

Summary


Details

When Extruding a one degree Spline, a Convergent body is the result instead of a Solid Body.

Solution

This is the result of the Modeling Preferences set.  To avoid this, edit the Modeling Preference toggling OFF the "Treat Degree 1 Spline as Polyline" on the Convergent tab.




Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DESIGN
Version: V12.0.2
Function: FEATURE_MODEL

Ref: 002-8008620

KB Article ID# PL8008620

Contents

SummaryDetails

Associated Components