Robot configuration problem - No option to teach.

2021-10-07T00:01:29Z

Summary


Details

In RobotExpert, there is no option to teach.

Solution

In this instance, the problem was based on the motionparameter.e file. This file is located inside the COJT directory that is inside the Library, which is inside the SystemRoot.
If you look at the motionparameter.e file inside the COJT for your ABB robot, you will see it is a text file that you can open with a text editor.
The purpose for the .e file is to set the limitations for the robot. 

Example of a motionparameter.e file:

config_family      cf_over_head_neg;
joint_config_family      j3     joint_cf_elbow_up;
joint_config_family      j4     joint_cf_cos_pos;
default_turns j6 0 -180 ;
zone_define  sp_zone1  no_smooth;
zone_define  sp_zone2  dist    cartesian        12.5 ;
zone_define  sp_zone3  dist    cartesian        25.0 ;
zone_define  sp_zone4  dist    cartesian        50.0 ;
zone_define  sp_zone5  dist    cartesian       100.0 ;
zone_define  sp_zone6  dist    cartesian       200.0 ;
zone_define  sp_zone7  dist    cartesian       300.0 ;
zone_define  sp_zone8  dist    cartesian       400.0 ;
zone_define  sp_zone9  dist    cartesian       500.0 ;
cart_max_lin_speed  1500;
cart_basic_lin_speed 1500;
interpolation_type  interpolate_by_3_j;



Notes and References

In this situation, the motionparameter.e file was completely missing.

Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: TECNOMATIX
Application: ROBOTEXPERT
Version: V14.1
Function: ROBOTICS

Ref: 002-8008603

KB Article ID# PL8008603

Contents

SummaryDetails

Associated Components