Model data is not being downloaded to cache when opening draft files.

2021-10-06T23:54:06Z

Summary


Details

When opening draft files from Teamcenter, the model data is not being downloaded to the local cache.

Solution

 This can occur when the Solid Edge client applications are installed using a login that is associated to a temporary profile.  This in turn causes some registration failures during the install. 

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V109MP12
Function: SEEC

Ref: 002-8008585

KB Article ID# PL8008585

Contents

SummaryDetails

Associated Components