Details
The display string attribute value is different after saving the template part file
Display string attribute is mapped between NX and TC.
User has created the template part file and imported into TCIN.
Value of the display string is correct and the issue starts if the template part file is opened in TCIN and saved.
Solution
Part file will be modified with attributes only when part is loaded and saved again.
So DisplayString attribute is computed differently before/after save.
Before save, mapped attribute is not present in part file so DisplayString is displayed as computed value in angular brackets, after template save when part is created this DisplayString is picked up from PART file and it will have different value i.e. same as mapping done.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: ATTRIBUTES
Ref: 002-8008584