What is the difference between tc_publishing_utility and ugtopv?

2021-10-06T23:26:37Z

Summary


Details

What is the difference between tc_publishing_utility and ugtopv?



Solution

ugtopv : You can use the command line application ugtopv for writing JT files from a selected set of .prt files. You can execute it directly from the NX command prompt or use a startup script to launch the ugtopv application.


tc_publishing_utility : You can use the tc_publishing_utility command line utility to publish NX part data to Teamcenter. The utility opens the part or assembly, publishes the data to Teamcenter, and then closes the part. Only metadata is published to Teamcenter. The part itself is not saved.
The following are supported for Teamcenter data publishing:
Feature publishing
Datum location
Product interfaces
Publish weld data option (the listed welds are published)
  Spot welds
  Arc welds
  Welding joints
  Surface welds


JT creation (synchronous and asynchronous)
Generating TrueShape
Drawing relations
Record part data
Recorded Altrep notes

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 1064
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: UTILITIES

Ref: 002-8008579

KB Article ID# PL8008579

Contents

SummaryDetails

Associated Components