Plant Simulation License for launching and running Plant from Excel

2021-10-07T00:01:29Z
Plant Simulation

Summary


Details

Are there any requirement of license for launching and running Plant from Excel :
1) Is InterfacePackage necessary to start and execute Plant Simulation from Excel ?
2) Is InterfacePackage necessary to start and execute Plant Simulation from applications developed in C language?
3) When InterfacePackage is used once, when will InterfacePackage be released?




Solution

In general the Interface Package is not needed for the communication with Excel.
To answer above specific three questions :

1) The Interface Package is not required to start Plant Simulation from Excel or from any other application.

2) See point1. As long as the application (developed in C or any other language) communicates via the COM Interface with Plant Simulation, the Interface Package is not required. If the C Interface is used, the Interface Package is required. The C Interface can load a DLL developed in C or C++ and communicate with it.

 3) All licenses are released when Plant Simulation is being closed. Closing the model will not release the licenses.



Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: TECNOMATIX
Application: PLANTSIMULATION
Version: V13.0
Function: ALL

Ref: 002-8008548

KB Article ID# PL8008548

Contents

SummaryDetails

Associated Components

Application Education Gantt Chart General Interface Package Professional Runtime Standard VSM Library