If "Carry Part Away" is missing in the exit strategy, how can it be used ?

2021-10-07T00:01:29Z

Summary


Details

Version : Tecnomatix Plant Simulation version 14.2.1533
It seems that "Carry Part Away" is missing in the exit strategy of Plant Simulation software.
It was present in prior versions of Plant Simulation.
How do use this particular feature ?



Solution

There is a change from Plant Simulation V14.2.

In 14.2 you can combine the exit strategies with transporting the part with a worker.
Therefore you need to configure the worker as a transport importer under the Importer tab.




Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: TECNOMATIX
Application: PLANTSIMULATION
Version: V14.2
Function: ALL

Ref: 002-8008544

KB Article ID# PL8008544

Contents

SummaryDetails

Associated Components