NX Is there a mom variable that stores whether a wedm op is 2 or 4 axis

2019-04-18T18:19:12Z
NX for Manufacturing

Summary


Details

Is there a system variable that the post is aware of so it can tell whether the current Wire EDM operation is defined as using 2 or 4 axis geometry? 

Solution

It should be possible to use the "mom_tool_axis_type" variable to test on what kind of wire path was defined in the operation. 

In a 2-axis wire operation, this has a 0 value. 

In a 4-axis wire operation, it does have a value of 4. 

A basic example of logic structure that can test on this variable in a custom command or an output condition in the post would look like:

======================================== 

global mom_tool_axis_type

if { $mom_tool_axis_type == 4 } { 

 set up the 4-axis stuff... 

 } else { 

 do the 2-axis stuff... 

 } 

========================================

Post writers can build any needed output or codes based on this framework. 

Notes

KB Article ID# PL8008530

Contents

SummaryDetails

Associated Components

Manufacturing Post Builder