Details
When revising a part that has the following name: aaaaa_001.par, Insight creates a file named aaaaa_001_1.par instead of aaaaa_002.par.
Solution
This will occur if the maximum character length for a revision is set to "2". Change it to "3" and this allows for correct revision values to be written. This setting is on the Solid Edge Settings -> Options, Manage page.
Hardware/Software Configuration
Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP6
Function: INSIGHT
Ref: 002-8008520