Teamcenter RAC is displaying a cyclical tree for Solid Edge Draft data sets

2021-10-06T23:54:04Z

Summary


Details

When displaying Item Revisions that contain a Solid Edge Draft data set in the Teamcenter RAC, there is a cyclical display under the draft data set.  It is starting with the Item Revision and continues expanding indefinitely.

Solution

 This is a preference setting in the Teamcenter RAC causing this behavior.  To disable this you need to select Edit/Options from the Teamcenter RAC interface and search for the preference "SE Draft_DefaultChildProperties".  Edit and remove the entry for "SE interpart Draft Links" 

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP8
Function: SEEC

Ref: 002-8008518

KB Article ID# PL8008518

Contents

SummaryDetails

Associated Components