Write access error message being returned on a Solid Edge assembly

2021-10-06T23:54:03Z

Summary


Details

Have a particular assembly that will not check out from Teamcenter. It is returning the following error message:  "The "Write" access is denied on the object "SE_Attr0" of class FormImpl (Form).  The access is denied.  The object "SE_Attr0" could not be loaded or refreshed. Please refer to the preceding errors in this error stack for more information."

Solution

To overcome this problem, check out the Solid Edge data set in the Teamcenter RAC.  After it is checked out, open the Named References for the data set and select to delete the SE_Attr0 form.  Then reopen the Solid Edge assembly, save and checked it in.  This recreates the SE_Attr0 form.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP8
Function: SEEC

Ref: 002-8008514

KB Article ID# PL8008514

Contents

SummaryDetails

Associated Components