Error message when attempting to import Solid Edge templates to Teamcenter

2021-10-06T23:54:03Z

Summary


Details

During the import Solid Edge templates, the following error message is returned:

"An unexpected error occurred while importing the Solid Edge templates.  Correct the issue using the information captured in the log file and then import your templates.

Solution

This could happen if the SEEC_ItemTypeList_* preferences, defined for each of the Solid Edge file types, contain a value of "All".  Edit each of the SEEC_ItemTypeList preferences and remove the "All" entry.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: DOC_MANAGEMENT
Version: V110MP10
Function: SEEC

Ref: 002-8008512

KB Article ID# PL8008512

Contents

SummaryDetails

Associated Components