Pointing to a common roles directory

2021-10-06T23:26:37Z

Summary


Details

How do you point to a common location for Roles?

Solution

Set the following variable:

UGII_USER_PROFILE_DIR = <path>
Enter the path to the folder where the "user.mtx" is located.

The variable UGII_USER_PROFILE_DIR will allow users to read and write to a user.mtx file placed in the location pointed to by this variable.

If user defined roles are not created then a "Roles" subdirectory is created at the location pointed to by the variable.


Also, you could use this.  This will not need a user-defined directory.  It uses the NX default directory and points to a specific file in that directory:

UGII_DEFAULT_ROLE = <file>.mtx

Note: The mtx file must be placed in the ugii\menus\roles directory for this variable to work.




Hardware/Software Configuration

Platform: na
OS: n/a
OS Version: n/a
Product: NX
Application: SYSENG
Version: V11.0
Function: UI_TOOLS

Ref: 002-8008475

KB Article ID# PL8008475

Contents

SummaryDetails

Associated Components