Part Utility command is not updating and saving UGMaster .prt data in Teamcenter

2021-10-06T23:26:37Z

Summary


Details

When running the part_utility.exe command with the -managed_mode=yes to perform actions on NX parts in Teamcenter the .prt file is not being updated and saved in Teamcenter?

Solution

There are two types of options within the part_utility.exe command. Some are non-part-modifying and some which are part-modifying. If both types are using in same command line the NX .prt file will not be saved back to Teamcenter.
This is intentional to avoid possible data corruption when using the various combinations and permutations of the part utility options.

Examples of non-part-modifying options are:
-record_part_data
-generate_trueshape
-record_altrep_notes

Examples of part-modifying options are:
-regen_lw
-convert_units_to_xxx
-convert_line_widths

For example if the following command line was used the .prt file in the named references would be updated (only using part-modifying options):

part_utility.exe -managed_mode=yes -u=xxx -p=xxx -i=C:\temp\list_of_parts.txt -regen_lw -y

If the additional option -record_part_data=yes (non-part-modifying option) is added to the same command the .prt file will no longer be updated. Only the record_part_data action will complete and the .prt file in Teamcenter will not be updated.

part_utility.exe -managed_mode=yes -u=xxx -p=xxx -i=C:\temp\list_of_parts.txt -regen_lw -y
-record_part_data=yes


The recommendation is to not mix part-modifying and non-part-modifying options within the same part_utility.exe command line.




Notes and References

Full list of options available for the part_utility.exe command can be found in the NX help documentation:

https://docs.plm.automation.siemens.com/tdoc/nx/1847/nx_help#uid:index_tcint:id1299838:xid1484425:xid1483666



Hardware/Software Configuration

Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: UTILITIES

Ref: 002-8008435

KB Article ID# PL8008435

Contents

SummaryDetails

Associated Components