Solid Edge Can not select faces with the Manual Connector command in Solid Edge Simulation.

2021-10-06T23:54:01Z
SIMULATION

Summary


Details

Faces are not selected with the Manual Connector command.

Solution

This can happen if you did not select the components with the 'Define Geometry' command.  You can click on 'Define Geometry'. The selected components will highlight. You can then click on the components you want to add.

Hardware/Software Configuration

Platform: INTL64
OS: window
OS Version: n/a
Product: SOLID_EDGE
Application: SIMULATION
Version: V219.0
Function: CONNECTORS

Ref: 002-8008389

KB Article ID# PL8008389

Contents

SummaryDetails

Associated Components

SIMULATION: ALL