How to remove precise save structure if saved using set precise on save

2021-10-06T23:26:36Z

Summary


Details

In NX, assembly is saved  after setting "Set Precise on Save".
Now user wants to undo the save operation.
He also want to hide this context menu option "Set Precise on Save"

Solution

It's not possible to hide "Set Save on Precise".


You can unset the precise save by following below method.
When you save an assembly by setting "Precise on Save", it saves the assembly with precise structure.
You can verify it in NX, in Assembly Navigator column "Precise Structure" it shows "Precise" Icon against the component nodes.
In TC, send the assembly to structure manager, all the nodes will be shown in "Green Color" to indicate precise structure.
You can unset the precise structure in TC, in structure manager, expand all the nodes & select them, now select Edit > Toggle Precise/ Imprecise.
This will make the assembly structure as imprecise and green color will be removed.
Similarly in NX, Assembly Navigator column "Precise Structure" will show "empty" against component nodes.(removing the precise icon)



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: NXMANAGER
Version: V12.0.2
Function: FILE_SAVE

Ref: 002-8008383

KB Article ID# PL8008383

Contents

SummaryDetails

Associated Components