NX Meaning of the switch "-env" (Specifying the customer environment for the part) in part_utility

2021-10-06T23:26:36Z
NX for Design

Summary


Details


What is the meaning of the switch "-env" in part_utility

Solution

This option is used while specifying different NX environment setups at cutomer sites.

An user like, a supplier who is dealing with multiple customers with different NX versions, can set up multiple NX environments at his site.
He maintains different Environment specific parts.
So while dealing parts with different NX environments, like while refiling "-env" switch is used to specify the NX environment.


The format is -env=<environment Name>


Please refer the below link related to creating NX environments in Teamcenter.
http://lmdbuild/tdoc/nx/12.0.2/nx_help#uid:index_tcint:id1299396:xid1411372



Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764
Product: NX
Application: NXMANAGER
Version: V1847
Function: UTILITIES

Ref: 002-8008377

KB Article ID# PL8008377

Contents

SummaryDetails

Associated Components

Teamcenter Integration for NX