Problem on Solid Edge ST8 Revision Manger when launching on Windows 10.

2021-10-06T23:54:00Z

Summary


Details

Problems in Revision Manager for Solid Edge ST8 MP12 on Windows 10 OS. 
Use can launch Revision Manager using a Solid Edge markup and tools it will launch but then it will close the part or assembly without being revised. Getting error message as mentioned below;
"SEVControl
Error starting the VisView application. Ensure the product is installed correctly."
 
User is able to run Revision Manager manually by right clicking on assembly file and  run with Revision Manager. 

Solution

1. Turn off User Account Control (UAC) on or off in Windows 10.
 
To turn User Account Control (UAC) off in Windows 10:
- Type UAC in the search field on your taskbar. (If the search field isn't visible, right-click the Start button and choose Search.)
- Click Change User Account Control settings in the search results.
- Then do one of the following:
- To turn UAC off, drag the slider down to Never notify and click OK.
- You may be prompted to confirm your selection or enter an administrator password.
- Reboot your computer for the change to take effect.
 
2. If this didn't helped then you need to reinstall Solid Edge ST8 with MP12 on any other drive e.g. 'D:' or 'E:' i. e. other than C: (the default install location).

Notes and References

9378227

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 10_1709
Product: SOLID_EDGE
Application: INSIGHT_CONNECT
Version: V108MP12
Function: VIEW_AND_MARKUP

Ref: 002-8008327

KB Article ID# PL8008327

Contents

SummaryDetails

Associated Components