What does the scale command do in draft?

2021-10-06T23:54:00Z

Summary


Details

What does the scale command do in draft?

Solution

The scale command reduces or enlarges selected elements by a scale factor that you define. The scale factor is the same along the x and y axes. Scalable elements include framed elements, such as text boxes. You can use the Scale command to scale, or to simultaneously scale and copy.





Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: MOLD_TOOLING
Version: V219.0
Function: MOLD_TOOLING

Ref: 002-8008309

KB Article ID# PL8008309

Contents

SummaryDetails

Associated Components