Making parting face flush with the Mold Plates

2021-10-06T23:53:59Z

Summary


Details

The parting face of the core and cavity blocks are not flush with the mold
plates.  How do you fix this?

Solution

Right-click your top level Parting Zone in the Mold Tooling tab in Edgebar and choose the Edit Dimensions command.  Click the "Thickness Step," then set the "Opening Point" (keypoint icon) option.  Graphically select a keypoint on your core or cavity block that is where the mold separates. This will align the plates parting zone with the blocks parting zone.

Hardware/Software Configuration

Platform: INTEL
OS: window
OS Version: 764SP1
Product: SOLID_EDGE
Application: MOLD_TOOLING
Version: V219.0
Function: MOLD_TOOLING

Ref: 002-8008305

KB Article ID# PL8008305

Contents

SummaryDetails

Associated Components