Creating a Reference Subop in a Generic Motion Operation

2021-10-06T23:26:36Z

Summary


Details

When selecting "Add New Sub-Operation", Reference Subop is not in the listing as "Move Type".


Solution

  • MB3 on the Generic Motion operation.
    • Select 'Object-->Customize'.
      • In the Items Used group, expand Sub-Operation Manager.


        • Select Reference Subop --> Customize Sub Dialog.


          The Customize Sub Dialog box will open.

          • Add the desired Dialog Item Type to the Items Used group (see image below).


            • Upon adding the desired types, select OK from the "Customize Sub Dialog" dialog box.

              It will return back to the main dialog box for the operation.

              •  Select the Name of the operation in the "Sub-Operations" group and then select  "Add New Sub-Operation"  (see image below).


                • Reference Subop now appears on the listing.


                  Notes

                  KB Article ID# PL8008290

                  Contents

                  SummaryDetails

                  Associated Components