Solid Edge Solid Edge 2019 - Maintenance Pack 5 Announcement

2021-10-07T00:10:00Z
SE_BETA SE_TSS DOC_MANAGEMENT FLOEFD 3D-SKETCH SIMULATION Teamcenter Share TECH_PUB ASSEMBLY APPLICATION PART/SHEETMETAL TRANSLATORS DRAFT SETUP

Summary


Details

March 7, 2019
 
Dear Solid Edge Customer: 
 
Solid Edge 2019 Maintenance Pack 5 is now available for download.
 
Sincerely,
The Solid Edge Team 
 
============
Release Notes:
============
 
Solid Edge 2019 Maintenance Packs are delivered using Microsoft Installer (MSI) technology.
 
Microsoft Windows 10 releases Feature Updates every six months. Microsoft does not use Windows 10 Feature Updates as an avenue to deliver security-related patches. All quality-related patches, including security and reliability hot-fixes, will continue to be delivered outside of this Feature Update process. Therefore, if your production use of Solid Edge was negatively impacted as a result of the last Microsoft Windows 10 Feature Update, you should consider configuring your Windows 10 machines to delay the deployment of Windows 10 Feature Updates. Configuring your Windows 10 machines by moving the machines into the "Semi-Annual Channel" servicing channel will delay the installation of Feature Updates for approximately four months following the initial release. During this time, you and your IT organization will have the opportunity to review the suitably of the Feature Update, including determining any negative impact, upon the applications that you use in your production environment, such as Solid Edge. This four-month window of time between Microsoft initially releasing the Feature Update to targeted machines and releasing the Feature Update for general deployment to the enterprise will also provide our development team time to review and react to changes introduced by Windows 10 Feature Updates, thereby helping keep you as productive as possible.
 
=====================
Maintenance Pack Version:
=====================
 
Solid Edge 2019 MP5
Version: 219.00.05.07
 
================
Download Location:
================
 
Solid Edge 2019 Maintenance Packs can be downloaded from:
 
   https://download.industrysoftware.automation.siemens.com/solid_edge/2019/Maintenance_Packs/
 
==========
Installation:
==========
 
  • MSI Product Updates can be applied on top of the base release and or existing Product Update with a lesser version.
  • MSI Product Updates are all inclusive, i.e. fixes delivered in MP3 include all fixes delivered in MP1 and MP2.
  • MSI Product Updates calculate free disk space before installing. Please be patient.
  • MSI Product Updates are uninstalled via the Control Panel (Uninstall a program –> View installed updates -> Uninstall).
  • MSI Product Updates can be uninstalled without having to remove the base Solid Edge product.
  • Uninstalling an MSI Product Update will restore the installation to the state before the Product Update was applied.
  • When uninstalling, the original source media must be available to allow the recovery of previous file versions.
  • The current MSI Product Update will be the only Update listed and available for uninstallation. 
  • After the current Product Update is uninstalled the previous Product Update will become the current Update.
  • .zip files delivered with this MP such as SEECAdministratorV219.zip are complete product setups. Therefore, existing versions of these installs must be removed using Uninstall a program from the Control Panel before installing the new version.
 
===============
E-mail Notification: 
===============
 
To receive direct e-mail notifications for new Solid Edge Maintenance Packs, subscribe to the SFBmail notification.
 
For details on initiating your email subscription navigate to: 
https://www.plm.automation.siemens.com/global/en/support/email-subscription.html
 
=========================================
This Maintenance Pack addresses the following PRs:
=========================================
 
===General=== 
PR 9325360: Solid Edge 2019 License Borrowing utility will not start Win 10 1803 and 1809
PR 9351038: SEHarnesspropseed.txt not found in non-English environment
 
===API===
PR 9134385: Add new part to assembly, save to QSM, part hidden, Undo, system error.
 
===Assembly=== 
PR 9119041: "Engineering reference" (Compensation gear design problem)
PR 9310980: Wrong size nuts and should screws are being generated in some cases
PR 9316364: Cannot change length and suppression variable together
PR 9195881: Unable to exclude parts in assembly copy
PR 9309628: Saving an assembly moves parts incorrectly
PR 9241501: Zero values and incorrect units for 'Moment of Inertia'
PR 8390233: Frame Recompute performance issues
PR 9337018: Solid Edge crashes while creating a splice on the bundle in below workflow
PR 9339646: several modeless dialogs not being destroyed correctly
PR 8555041: When I use "Project To Sketch", "highlight" is not working normally 
PR 9329260: Crash when reordering multiple group items into another group
 
===Draft=== 
PR 9292023: Independent Detail Views go out of date by viewing a different sheet
PR 9332974: mass property text now is blank in drafts.
 
===Part/Sheet Metal===
PR 9075662: Unable to uncheck 'Use Excel File' from Gage Properties
PR 9308215: Solid Edge Standard parts Generating always hang up & Crashing 
PR 9308280: Empty pitch values in DB for Hole command in SE 2019
PR 9320080: Mass of Generative Design part is 0 if saved before the generation
PR 9265929: Editing synchronous thread pitch value changes thread size
PR 9018880: Cannot make Sync edit on Sheet Metal if another part was edited and closed
PR 9323165: Pitch is grossly wrong when using Saved Settings
PR 9340182: Cannot use drag and drop to place block in sketch
PR 9310743 : Non-stitched edges are not highlighted behind another face 
PR 9352885: Sheet metal file aborts when flattened
 
===Translators===
PR 8329150: Dimension lines are not trimmed when importing this DXF file
PR 9253967: Solid Edge crashed while open JT data
PR 9290085: Multi body does not show up in Parasolid conversion
PR 9285318: adding a cut into a mesh model prevents Local 3D printing from working
PR 9214451: Legacy JT translator takes significantly less time than current JT translator
 
===Design Manager===
PR 9295553: 'Expand All: Populate duplicates' does not persist if you check 'Don't show'
PR 9295035: Revise dataset creates incorrect revision history for some parts
 
===Teamcenter Integration for Solid Edge===
PR 9315592: Project assign is cleared when uploading without displaying the CPD
PR 9315778: Switching "Show View" to "Parts List" in SESE aborts  
PR 9339186: SolidEdgeTranslationServices will not generate flat pattern DXF for .par file 
PR 9241966: Problems installing Solid Edge Templates
PR 9323959: Preference SEEC_Enable_MultipleRevision=1 breaking Solid Edge links.
PR 9309476: Project update on other user data is displaying an error message in Solid Edge

SFB-SOLID_EDGE-8008285
Product Information:
  • Product: SOLID_EDGE

KB Article ID# PL8008285

Contents

SummaryDetails

Associated Components

SE_BETA