When selecting a dimension command in the Drafting application, the following error is reported:
Error opening limit fit data files.
Solution
This error can mostly be caused by two situations:
1. The UGII_DRAFTING_STANDARD_DIR variable is not set correctly.
· Solution: Set this variable to point to the correct location.
2. The UGII_DRAFTING_STANDARD_DIR is set correctly, but missing files.
· Solution: Custom location may be missing files. Copy the sub-folders from "%UGII_BASE_DIR%\UGII\drafting standards" into the custom location.
Notes and References
Hardware/Software Configuration
Platform: all
OS: n/a
OS Version: n/a
Product: NX
Application: DRAFTING
Version: V11.0.2
Function: DIMENSION
Ref: 001-9386673